EtherNet/IP™ Adapter3.02.00

Overview

The basic API functions cover general functionality such as creating, initializing, starting, and deleting an EtherNet/IP adapter object. The adapter object is a required input parameter for all other adapter API functions. Also supported are API functions to retrieve the adapter status and to register status and error handler callback functions.

Functions

uint32_t EI_API_ADP_pruicssInit (EIP_SLoadParameter *ptPara_p)
 Load and initialize the EtherNet/IP firmware in the PRU. More...
 
void EI_API_ADP_pruicssStart (void)
 Starts the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit. More...
 
void EI_API_ADP_pruicssStop (void)
 Stops the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit. More...
 
T * EI_API_ADP_new (uint8_t numInterfaces_p)
 Create a new EtherNet/IP adapter. More...
 
uint32_t EI_API_ADP_delete (T *pAdp_p)
 Delete an existing EtherNet/IP adapter. More...
 
uint32_t EI_API_ADP_init (T *pAdp_p, EI_API_ADP_SInit_t params_p)
 Apply parameters. More...
 
void EI_API_ADP_run (void)
 Main run function. More...
 
uint32_t EI_API_ADP_getModuleNetworkStatus (T *pAdp_p, EI_API_ADP_SModNetStatus_t *pAdpStatus_p)
 Get adapter status values. More...
 
uint32_t EI_API_ADP_setModuleNetworkStatusFunc (T *pAdp_p, EI_API_ADP_CBStatus callback_p)
 Handle module and network status changes. More...
 
uint32_t EI_API_ADP_setErrorHandlerFunc (EI_API_ADP_CBStackError callback_p)
 Set the stack error handler function. More...