|
AM64x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
52 #if defined (SOC_AM64x) || defined (SOC_AM243X)
53 #include <sdl/include/am64x_am243x/sdlr_soc_baseaddress.h>
54 #include <sdl/include/am64x_am243x/sdlr_mcu_ctrl_mmr.h>
106 typedef struct SDL_Pok_Static_Reg_read{
Header file containing various enumerations, structure definitions and function declarations for the ...
bool porBGapOK
Definition: pok/v1/sdl_pok.h:119
int8_t SDL_POK_Inst
Definition: sdl_pok_def.h:130
uint8_t hystCtrl
Definition: pok/v1/sdl_pok.h:107
POK Configuration structure.
Definition: sdl_pok_def.h:420
int32_t SDL_POK_getStaticRegisters(SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
int8_t SDL_PRG_Inst
Definition: sdl_pok_def.h:129
POK Static Registers structure.
Definition: pok/v1/sdl_pok.h:106
This file contains the SDL DPL API's.
uint8_t hystCtrlOV
Definition: pok/v1/sdl_pok.h:109
uint8_t trimOV
Definition: pok/v1/sdl_pok.h:115
int32_t SDL_POK_verifyConfig(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK Function to verify the written configuration. This function checks the provided config against th...
uint8_t trim
Definition: pok/v1/sdl_pok.h:113
uint8_t voltDetMode
Definition: pok/v1/sdl_pok.h:111
uint8_t deglitch
Definition: pok/v1/sdl_pok.h:117
uint8_t porModuleStatus
Definition: pok/v1/sdl_pok.h:121
int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable)
POK Function to enable or diable ping/pong mode for a specified PRG. Only supported for v1 version of...
int32_t SDL_POK_init(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK module configuration API.
@ enable
Definition: iPtcpDrv.h:69