AM64x MCU+ SDK  08.06.00
MCSPI Migration Guide

This section describes the differences between MCSPI APIs of MCU+ SDK and Processor SDK RTOS (PDK). This can be used as a migration aid when moving from Processor SDK RTOS (PDK) to MCU+ SDK.

In MCU+ SDK, the MCSPI module provides both low latency and higher level driver APIs.Refer MCSPI for more details. From the user point of view, higher level API usage is same as in PDK.APIs name begins with MCSPI_ instead of SPI_. Low latency APIs are provided on top of these higher level abstracted APIs and the usage of these APIs are showcased in MCSPI Performance 8 Bit example.

API changes

There are changes in API names, structure names and macro names. Low latency API names also begin with MCSPI_ now. The low latency available API names and the name changes are listed below.

PDK MCU+ SDK Remarks
McSPIClkConfig MCSPI_chConfig Configuring field MCSPI_ChConfig::bitRate in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPIWordLengthSet MCSPI_chConfig Configuring field MCSPI_Transaction::dataSize in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPICSEnable MCSPI_open CS is enabled via SysConfig.
McSPICSDisable MCSPI_open CS is disabled via SysConfig.
McSPICSPolarityConfig MCSPI_chConfig Configuring field MCSPI_ChConfig::csPolarity in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPICSTimeControlSet MCSPI_chConfig Configuring field MCSPI_ChConfig::csIdleTime in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPICSAssert MCSPI_writeChConfReg In MCU+SDK CS is asserted by driving FORCE field using MCSPI_writeChConfReg.
McSPICSDeAssert MCSPI_writeChConfReg In MCU+SDK CS is asserted by driving FORCE field using MCSPI_writeChConfReg.
McSPIStartBitEnable MCSPI_open Configuring field MCSPI_ChConfig::startBitEnable in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPIStartBitPolarityConfig MCSPI_open Configuring field MCSPI_ChConfig::startBitPolarity in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPIStartBitDisable MCSPI_close
McSPIControllerModeEnable MCSPI_open Configuring field MCSPI_OpenParams::msMode in MCSPI_OpenParams will do the equivalent of PDK MCSPI API.
McSPIPeripheralModeEnable MCSPI_open Configuring field MCSPI_OpenParams::msMode in MCSPI_OpenParams will do the equivalent of PDK MCSPI API.
McSPIControllerModeConfig MCSPI_open MCSPI_chConfig Configuring fields MCSPI_Attrs::chMode,MCSPI_Attrs::pinMode in MCSPI_Attrs, field MCSPI_ChConfig::trMode in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPIChannelEnable MCSPI_writeChCtrlReg In MCU+SDK Channel is enabled by setting EN field using MCSPI_writeChCtrlReg.
McSPIChannelDisable MCSPI_writeChCtrlReg In MCU+SDK Channel is enabled by clearing EN field using MCSPI_writeChCtrlReg.
McSPIReset MCSPI_open
McSPITurboModeEnable None In MCU+SDK API not supported
McSPITurboModeDisable None In MCU+SDK API not supported
McSPITxFIFOConfig MCSPI_enableTxFIFO Only API name change
McSPIRxFIFOConfig MCSPI_enableRxFIFO Only API name change
McSPIFIFOTrigLvlSet MMCSPI_open In MCU+SDK, FIFO trigger level is set to fixed value based on transfer mode.
McSPIWordCountSet MCSPI_transfer
McSPIDMAEnable None In MCU+SDK API not supported
McSPIDMADisable None In MCU+SDK API not supported
McSPIIntEnable MCSPI_transfer
McSPIIntDisable None Interrupt mode is supported only in higher level driver APIs and driver manages ISR.
McSPIInitDelayConfig MCSPI_open Configuring field MCSPI_Attrs::initDelay in MCSPI_Attrs will do the equivalent of PDK MCSPI API.
McSPITransmitData MCSPI_writeTxDataReg Only API name change
McSPIReceiveData MCSPI_readRxDataReg Only API name change
McSPIIntStatusGet None Interrupt mode is supported only in higher level driver APIs and driver manages ISR.
McSPIIntStatusClear None Interrupt mode is supported only in higher level driver APIs and driver manages ISR.
McSPIChannelStatusGet MCSPI_readChStatusReg Only API name change
McSPIMultipleWordAccessConfig None In MCU+SDK API not supported
McSPIFIFODatManagementConfig None In MCU+SDK API not supported
MCSPISysConfigSetup MCSPI_open
MCSPIPinDirSet MCSPI_open Configuring field MCSPI_ChConfig::inputSelect, MCSPI_ChConfig::dpe0 and MCSPI_ChConfig::dpe1 in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
MCSPISingleChModeEnable MCSPI_open Configuring field MCSPI_Attrs::chMode in MCSPI_Attrs will do the equivalent of PDK MCSPI API.
MCSPIMultiChModeEnable MCSPI_open Configuring field MCSPI_Attrs::chMode in MCSPI_Attrs will do the equivalent of PDK MCSPI API.
McSPISetPeripheralChipSel MCSPI_open Configuring field MCSPI_ChConfig::slvCsSelect in MCSPI_ChConfig will do the equivalent of PDK MCSPI API.
McSPIGetChannelCtrl MCSPI_readChCtrlReg Only API name change
McSPISetChannelCtrl MCSPI_writeChCtrlReg Only API name change
McSPIGetChannelConf MCSPI_readChConf Only API name change
McSPISetChannelConf MCSPI_writeChConfReg Only API name change
Not Available MCSPI_getBaseAddr This API is only present in MCU+SDK
Not Available MCSPI_reConfigFifo This API is only present in MCU+SDK
Not Available MCSPI_getBufWidthShift This API is only present in MCU+SDK

Important Notes

  • In MCU+ SDK, Users are recommended to use SysConfig as this will greatly simplify the task of driver configuration. SysConfig can be used to configure below parameters for both low latency and higher level driver usage.
  • MCSPI module configuration parameters like Transmit/Receive mode, MISO, MOSI pin selection, Clock config,Setting word length and others.
  • MCSPI channel configurations like CS enable, CS Polarity, CS Time Control and others.
  • In the advanced configurations option you can configure initial delay for first transfer, transfer mode and timeout.
  • MCSPI instances and pin configurations.
  • Interrupt enable/disable.
  • To use low latency APIs user should follow below steps.
    • User should configure "Interrupt mode enable" option in SysConfig to "Polling"
    • User should get the base address of MCSPI module by calling MCSPI_getBaseAddr API.
    • This base address should be used to call low latency APIs.
    • Please refer MCSPI Performance 8 Bit example for the usage of low latency APIs.

See Also