AM64x MCU+ SDK  08.06.00
IO-Link Controller Demo

Introduction

This example is an IO-Link controller application based on evaluation stack provided in the SDK. Links to important sections in the detailed documentation are provided below:

IO-Link Controller GUI Tool can be downloaded from here.

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG0
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/industrial_comms/iolink_master_demo