uint16_t EC_SLV_APP_AoE_readRequest | ( | void * | pContext_p, |
uint16_t | port_p, | ||
uint16_t | index_p, | ||
uint8_t | subIndex_p, | ||
bool | completeAccess_p, | ||
uint32_t * | pLength_p, | ||
uint16_t * | pData_p | ||
) |
AoE read request handler.
[in] | pContext_p | The pointer to the EtherCAT API instance. |
[in] | port_p | AMS port. |
[in] | index_p | 16 bit index value from IndexOffset. |
[in] | subIndex_p | 8 bit subIndex value from IndexOffset. |
[in] | completeAccess_p | CoE Complete Access flag. |
[in,out] | pLength_p | Request data length. |
[in] | pData_p | Pointer to data. |