EtherCAT Slave1.11.00

◆ EC_API_SLV_FoE_cbRegisterFwUpdate()

void EC_API_SLV_FoE_cbRegisterFwUpdate ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_FoE_CBFwUpdateHandler_t  cbFunc_p 
)

This is the function to register FoE firmware update function.

This function registers a function pointer which must be implemented by the user. The user defined function will be called if a firmware update request is received from the master

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pContext_pfwUpdate call context
[in]cbFunc_pFunction pointer to the Firmware Update Handler
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_FoE_cbRegisterCloseFileHandler(ecSlaveApi, ecSlaveApi, cbFunc);
EC_API_SLV_FoE_cbRegisterCloseFileHandler
void EC_API_SLV_FoE_cbRegisterCloseFileHandler(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_FoE_CBCloseFileHandler_t cbFunc_p)
This is the function to register FoE close function.
Definition: ecSlvApi_FoEStub.c:208