![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
38 #ifndef RED_VLANTABLE_H_
39 #define RED_VLANTABLE_H_
127 uint16_t vid, uint8_t command);
RED_STATUS vlan_filter_config(PRUICSS_Handle pruicssHandle, uint8_t command)
set the VLAN_FLTR_CTRL_SHIFT to enable/disable vlan filtering
Commonly used Macros, structures and Offsets.
RED_STATUS
RED Status.
Definition: hsrPrp_red_common.h:526
RED_STATUS vlan_filter_update_vid(PRUICSS_Handle pruicssHandle, uint16_t vid, uint8_t command)
insert/delete a VID in the VLAN filter table
RED_STATUS vlan_untagged_frames_config(PRUICSS_Handle pruicssHandle, uint8_t command)
set the VLAN_FLTR_UNTAG_HOST_RCV_CTRL_SHIFT to enable/disable untagged frame host receive
RED_STATUS vlan_priotag_frames_config(PRUICSS_Handle pruicssHandle, uint8_t command)
set the VLAN_FLTR_PRIOTAG_HOST_RCV_CTRL_SHIFT to enable/disable priority frame host receive
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/g_v0/pruicss.h:235
Include file for hsrPrp_red_vlanTable.c.
RED_STATUS vlan_sv_frames_config(PRUICSS_Handle pruicssHandle, uint8_t command)
set the VLAN_FLTR_SV_CTRL_SHIFT for SV frames to skip/enter VLAN flow