C:/ti in Windows, and ${HOME}/ti in Linux. To install to other locations, refer Installing SDK at non-default location{some text} refers to a variable string that should be replaced by user and {some text} should not be typed verbatim on the command prompt.cmd.exe as command prompt and in Linux, use the bash shell as the command prompt.On successful completion of below steps, you would have achieved the following
| Term | Description |
|---|---|
| McSPI Controller | McSPI in communication which generates the clock and initiates the transfer |
| McSPI Peripheral | McSPI in communication which read and write data based on Controller clock |
| I2C Controller | I2C device which generates the SCL clock and initiates communication |
| I2C Target | I2C device which responds to I2C Controller |
| LIN Commander | LIN device which intiates the transfer |
| LIN Responder | LIN device which responds to the transfer |
| PTP Sync Time Source | Ethernet device that periodically broadcasts the current time as a message to the other clocks |
| PTP Sync Receiver | Ethernet device that is waiting for the master to poll for data to actually send it |
| EtherCAT MainDevice | EtherCAT device which is allowed to trasfer the data across network |
| EtherCAT SubDevice | EtherCAT device which reads the data addressed to them bu MainDevice |
| Ethernet/IP Scanner | Ethernet/IP scanned is the client device responsible for establishing a connection path to an EtherNet/IP Adapter |
| Ethernet/IP Adapter | Ethernet/IP adapter which receives implicit communication connection requests from an scanner then produces its I/O data at the requested rate. An adapter is also an explicit message server. |
| IO-Link Controller | IO-Link device which provides the interface to the higher-level controller (PLC) and controls the communication with the connected IO-Link devices. An IO-Link master can have one or more IO-Link ports to which only one device can be connected at a time |
| IO-Link Device | IO-Link device is a short distance, bi-directional, digital, point-to-point, wired (or wireless), industrial communications networking standard (IEC 61131-9) used for connecting digital sensors and actuators to either a type of industrial fieldbus or a type of industrial Ethernet |
Now you can explore the SDK by running more examples (see Examples and Demos) and browsing through various developer notes (see Developer Guides), to understand the SDK better and develop your own applications with the SDK.