AM64x MCU+ SDK  08.04.00
ADS127 Implementation Details

Implementation Details

The control of ADC pins is divided between PRU and R5F cores.

In example, the interfacing with ADS127L11 operates in following configuration:

  • 1.0677MSPS sampling rate
  • Continous sampling of data
  • Signal trace for the current implementation is shown in figure below (can check timing details from this)

R5F Function:

  • Send ADC register configuration information to the PRU core
  • Send instructions to PRU core
  • Wait for interrupt from PRU indicating 1 block of adc samples has been received
  • On interrupt fetch the block id to read and read the samples
  • Process them as needed
/* Total number of Commands to send to ADC */
uint16_t noOfCommands = 4;
/* Commands array
* Add your commands to this (maximum = noOfCommands)
*/
uint16_t adcConfigCommands[4] = {0x8708, 0x8708, 0x8708, 0x8708};
ADC_init();
ADC_powerUp();
ADC_configure(noOfCommands, adcConfigCommands);
ADC_startConversion();
/* Get ADC data from PRU */
PRU_IPC_getData(gPruIpc0Handle, samples);

PRU Function:

  • Wait for commands from R5F and do accordingly While executing ADC interface section:
  • Wait for ADC Busy to go low indicating conversion has completed
  • Start reading samples from each ADC channel
  • Preprocess samples as required
  • Send samples to shared memory using ipc
  • Repeat above steps again
START:
; Wait for DRDY to go low indicating conversion has completed
; DRDY: _᠆᠆᠆᠆_____________________________________________________
; SDI: _____| Status | < Channel 0 - 4 Data > | CRC |____
m_wait_high_pulse 2, DRDY_PIN
; Fetch samples using serial interface
m_wait_nano_sec 10
m_pru_clr_pin ADC_CS_PIN ; set CS low
m_wait_nano_sec 10
m_read_packet_spi_mode1_msb_iep_sclk ADC_DATA_REG_1, 24, R5.b0, TEMP_REG_1, 0, SDI_PIN, SYNC0, 15, 3
m_wait_nano_sec 10
m_pru_set_pin ADC_CS_PIN ; set CS high
m_sign_ext 24, 32, ADC_DATA_REG_1, EXTEND_0
ldi R1.b0, &ADC_DATA_REG_1
m_pru_ipc_send R1.b0, ADC_DATA_REG_1, R0.b0, R29, CONFIG_PRU_IPC0_RX_INTR_ENABLE, CONFIG_PRU_IPC0_RX_EVENT
m_prgm_flow_jump_on_intr PRGM_FLOW_EVENT, PRGM_FLOW_EVENT_BIT, 6, TEMP_REG_1, IDLE, IEP, SAMPLE_TRANSFER, ADC_CONFIG, READ_SAMPLES, RESET
qba START ; loop to continue collecting samples
halt
Tips to Modify PRU Firmware: Refer to PRU Source Macros Documentation for making changes to PRU firmware.