AM64x MCU+ SDK  08.04.00
UDMA SW Trigger

Introduction

UDMA SW trigger sample application performs 3D transfer using SW trigger method as below Loop N times (icnt2)

  • SW trigger CH 0 -> Triggers MSMC to Intermediate buffer
  • Wait for CH 0 icnt0 x icnt1 to complete
  • SW trigger Channel 1 -> Triggers Intermediate buffer to MSMC
  • Wait for CH 1 icnt0 x icnt1 to complete

Each loop transfers M (icnt0 x icnt1) bytes of data. MSMC size is M x N and intermediate buffer size is just M bytes. Intermediate buffer memory set to wrap around after M bytes of transfer.

Where,

  • M is icnt0 x icnt1 (UDMA_TEST_1D_SIZE x UDMA_TEST_2D_SIZE)
  • N is icnt2 = UDMA_TEST_3D_SIZE

Once the transfer it completes, it does cache operation for data coherency and compares the source and destination buffers for any data mismatch.

Supported Combinations

Attention
A53 NORTOS, A53 FREERTOS and A53 FREERTOS SMP support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 freertos
a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-0 freertos-smp
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/udma/udma_sw_trigger

Steps to Run the Example

See Also

UDMA

Sample Output

Shown below is a sample output when the application is run,

[UDMA] SW Trigger application started ...
All tests have passed!!