PROFINET Device  v2.01.00

◆ PN_API_DEV_getNumberOfExpectedModules()

uint32_t PN_API_DEV_getNumberOfExpectedModules ( PN_API_DEV_EAr_t  ar_p,
uint16_t *  pNumberOfModules_p 
)

Get number of expected IO device modules.

ToDo.

Parameters
[in]ar_pApplication relation.
[out]pNumberOfModules_pNumber of modules.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run