PROFINET Device  v2.01.00

◆ PN_API_DEV_setInputDataBuffer()

uint32_t PN_API_DEV_setInputDataBuffer ( uint8_t *  pAddr1_p,
uint8_t *  pAddr2_p,
uint8_t *  pAddr3_p,
uint16_t  bufferSize_p 
)

Set input data triple buffer of IO device.

ToDo.

Parameters
[in]pAddr1_pAddress of buffer 1 of triple buffer.
[in]pAddr2_pAddress of buffer 2 of triple buffer.
[in]pAddr3_pAddress of buffer 3 of triple buffer.
[in]bufferSize_pSize of buffer 1, 2, 3 of triple buffer.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run