This example just does driver and board initialization and prints the string, Hello World! on UART console.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
r5fss0-0 freertos | |
m4fss0-0 nortos | |
m4fss0-0 freertos | |
a53ss0-0 nortos | |
a53ss0-0 freertos | |
a53ss0-0 freertos-smp | |
Toolchain | ti-arm-clang |
arm.gnu.aarch64-none | |
Boards | am64x-evm, am64x-sk |
Example folder | examples/empty/ |
Shown below is a sample output when the application is run,