This is a special example which sends the sciclient boardcfg to the SYSFW running on Cortex M3. This example is mainly used in conjunction with the NO BOOT MODE, refer to SOC Initialization Using CCS Scripting for more information on this.
The boardcfg is a SOC specific configuration data regarding the various system attributes controlled by the SYSFW. These include resources, power and clock, security etc.
If the SYSFW accepts the boardcfg sent, the test result is passed otherwise failed.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am64x-evm, am64x-sk |
Example folder | examples/drivers/sciclient/sciclient_set_boardcfg |