This is a bootloader which does SOC initializations and put all the cores in WFI. This example is what is referred to as the SOC initialization binary in Flash SOC Initialization Binary. The SBL NULL does not load any images on the cores. For more information on how this example is being used, refer Flash SOC Initialization Binary
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am64x-evm, am64x-sk |
Example folder | examples/drivers/boot/sbl_null |
Since this is a bootloader and is used as a SOC initialization binary, the example will be run every time you boot an application using this example. It is generally run from a boot media (OSPI Flash, SD Card) unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.