AM64x MCU+ SDK  08.03.00
MCAN Loopback Interrupt

Introduction

This example demonstrates the CAN message transmission and reception in digital loop back mode with the following configuration.

  • CAN FD Message Format.
  • Message ID Type is Standard, Msg Id 0xC0.
  • MCAN is configured in Interrupt Mode.
  • MCAN Interrupt Line Number 0.
  • Arbitration Bit Rate 1Mbps.
  • Data Bit Rate 5Mbps.
  • Buffer mode is used for Tx and RX to store message in message RAM.

Message is transmitted and received back internally using internal loopback mode. When the received message id and the data matches with the transmitted one, then the example is completed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Board am64x-evm, am64x-sk
Example folder examples/drivers/mcan/mcan_loopback_interrupt

Steps to Run the Example

See Also

MCAN

Sample Output

Shown below is a sample output when the application is run,

[MCAN] Loopback Interrupt mode, application started ...
All tests have passed!!