The following sections describe the steps to configure projects that contain one PLC that implementing EtherNet/IP Scanner functionality and one SITARA AM64x based EtherNet/IP Adapter device.
Examples are provided for CODESYS IEC 61131 development and runtime environments executing on Texas Instruments AM64x evaluation boards (SK-AM64, TMDS64GPEVM), an industrial RevPi Connect hardware (https://revolution.kunbus.com/) by KUNBUS GmbH, and an Allen-Bradley CompactLogix L16ER PLC that is configured and programmed from the RSLogix 5000 development environment.
stc
directory was removed and replaced by a new soc
directory. The older configuration files in STC format are still retained in the soc
directory for compatibility reasons with ODVA test tools CT17 or earlier. EDS file(s) can be found in the following path: mcu_plus_sdk\source\industrial_comms\ethernetip_adapter\stack\eds
SOC file(s) required for the ODVA CT18.1 can be found in the following path: mcu_plus_sdk\source\industrial_comms\ethernetip_adapter\stack\soc
See CODESYS Runtime on a Texas Instruments AM64x Sitara Processor
See CODESYS Runtime on a KUNBUS RevPI Controller