typedef void(* EC_API_SLV_CBPhySpecific_rgmiiTxHalfFullThreshold_t) (void *pAppContext_p, void *pStackContext_p, uint32_t phyAddr_p, uint32_t threshold_p) |
RGMII_TX_HALF_FULL_THR[1:0] can be changed from the default of 0x2 to 0x1. This will reduce the latency by one clock period.
[in] | pAppContext_p | application context |
[in] | pStackContext_p | slave stack context |
[in] | phyAddr_p | phy address |
[in] | threshold_p | Number of cycles for threshold (2, 1) |