typedef void(* EC_API_SLV_CBStackError_t) (void *pAppRunCtxt_p, uint32_t errorCode_p, uint8_t fatal_p, uint8_t numOfParam_p, va_list arg_p) |
Called on severe Stack error (OSAL_error)
[in] | pAppRunCtxt_p | CallBack Content for use in complex applications. |
[in] | errorCode_p | Error code from DTK Stack |
[in] | fatal_p | Error type |
[in] | numOfParam_p | number of upcoming parameters |
[in] | arg_p | rest of parameters |