typedef bool(* EC_API_SLV_EoE_CBSettingIndHandler_t) (void *pContext_p, uint16_t *pMac_p, uint16_t *pIp_p, uint16_t *pSubNet_p, uint16_t *pDefaultGateway_p, uint16_t *pDnsIp_p) |
EoE Settings Indication callback proxy.
[in] | pContext_p | The pointer to the EtherCAT API instance. |
[in] | pMac_p | Virtual Net MAC address |
[in] | pIp_p | Virtual Net IP address |
[in] | pSubNet_p | Virtual Net Subnet |
[in] | pDefaultGateway_p | Virtual Net Default Gateway |
[in] | pDnsIp_p | Virtual Net DNS server address |