|
AM64x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
54 typedef struct PN_IntAttrs_s
77 typedef struct PN_IntConfig_s
87 #ifdef ENABLE_LATCH_SUPPORT
uint32_t intPrio
Definition: PN_Handle.h:64
Definition: PN_Handle.h:78
void * callBackPtr
Definition: PN_Handle.h:70
void * isrFnPtr
Definition: PN_Handle.h:68
struct PN_Config_s * PN_Handle
Alias for Profinet Handle containing base addresses and modules.
Definition: PN_Handle.h:96
uint32_t coreIntNum
Definition: PN_Handle.h:60
uint32_t pruIntNum
Definition: PN_Handle.h:58
uint32_t socEvId
Definition: PN_Handle.h:62
void * args
Definition: PN_Handle.h:66
PN_IntAttrs ptcpIntConfig
Definition: PN_Handle.h:86
Definition: PN_Handle.h:55
PN_IntAttrs dhtIntConfig
Definition: PN_Handle.h:84
PN_IntAttrs cpmIntConfig
Definition: PN_Handle.h:82
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:91
PN_IntAttrs ppmIntConfig
Definition: PN_Handle.h:80
HwiP_Object interruptObject
Definition: PN_Handle.h:56