Introduction
This is a flash-writer example which uses JTAG to write files or erase flash and thereby removes UART dependency. Although it is not strictly a bootloader, it uses flash APIs to be able to flash binaries to the OSPI/QSPI flash. This example performs the following operations.
- Flash the received file at the given offset
- Verify if the data in the received file is present at the given offset
- Erase the entire flash.
Once the example starts running it displays a following menu.
1: Erase Complete Flash
2: Write File to Flash and Verify
3: Verify file in Flash
x: Exit
Enter Choice:
After the file is written, verified or flash is erased, an acknowledgment is sent back to the console and the loop continues. This example is more or less like a flashing server, and will terminate until user does not enter 'x'.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am64x-evm |
Example folder | examples/drivers/boot/sbl_jtag_uniflash |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Before loading this program and run on the EVM, the SOC needs to be initialized. It is recommended to use the method mentioned in SOC Initialization Using CCS Scripting
- Attention
- Do not perform DDR Initialization DDR_INIT as it is done in the example itself.
- Reset the CPU and Load program on the CPU
See Also
BOOTLOADER
Sample Output
==================
JTAG Uniflash Menu
==================
1: Erase Complete Flash
2: Write File to Flash and Verify
3: Verify file in Flash
x: Exit
Enter Choice: 1
[FLASH WRITER] Erasing complete flash ...
[FLASH WRITER] This can take few minutes, so please wait ...
[FLASH WRITER] Erasing complete flash ... SUCCESS !!!
==================
JTAG Uniflash Menu
==================
1: Erase Complete Flash
2: Write File to Flash and Verify
3: Verify file in Flash
x: Exit
Enter Choice: 2
Enter file name along with path to write or verify : C:\Users\x0190988\Downloads\mcu_plus_sdk_08_02_00\tools\boot\sbl_prebuilt\am243x-evm\sbl_null.release.tiimage
Enter flash offset (in hex format) : 0x0
Enter below command in CCS scripting console to load the file data to memory.
AFTER the file load is done, enter '1' to continue ...
loadRaw(0x80000020, 0, "C:/Users/x0190988/Downloads/mcu_plus_sdk_08_02_00/tools/boot/sbl_prebuilt/am243x-evm/sbl_null.release.tiimage", 32, false);
1
[FLASH WRITER] Flashing success!!...
==================
JTAG Uniflash Menu
==================
1: Erase Complete Flash
2: Write File to Flash and Verify
3: Verify file in Flash
x: Exit
Enter Choice: 3
Enter file name along with path to write or verify : C:/Users/x0190988/Downloads/mcu_plus_sdk_08_02_00/tools/boot/sbl_prebuilt/am243x-evm/sbl_null.release.tiimage
Enter flash offset (in hex format) : 0x0
Enter below command in CCS scripting console to load the file data to memory.
AFTER the file load is done, enter '1' to continue ...
loadRaw(0x80000020, 0, "C:/Users/x0190988/Downloads/mcu_plus_sdk_08_02_00/tools/boot/sbl_prebuilt/am243x-evm/sbl_null.release.tiimage", 32, false);
1
[FLASH WRITER] Verifying success!!...
==================
JTAG Uniflash Menu
==================
1: Erase Complete Flash
2: Write File to Flash and Verify
3: Verify file in Flash
x: Exit
Enter Choice: x
[FLASH WRITER] Application exited !!!
All tests have passed!!