PROFINET Device
v1.04.03
◆
PN_API_DEV_registerReleaseResponseCallback()
uint32_t PN_API_DEV_registerReleaseResponseCallback
(
PN_API_DEV_releaseResponseCallback
cbFunction_p
)
Register IO device callback indicating a release response is to be sent.
ToDo.
Parameters
[in]
cbFunction_p
Callback function.
Returns
PN_API_DEV_EError_t
as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start
PN_API_PDEV_run
PROFINET Device API
generated by
1.8.18