|
typedef void(* | EI_API_CIP_CBService) (EI_API_CIP_NODE_T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, EI_API_CIP_ESc_t serviceCode_p, int16_t serviceFlag_p) |
| Function prototype for CIP service callback functions. More...
|
|
typedef uint32_t(* | EI_API_CIP_CBGetAttr) (EI_API_CIP_NODE_T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, uint16_t *len_p, void *pvValue_p) |
| Function prototype for CIP get attribute callback function. More...
|
|
typedef uint32_t(* | EI_API_CIP_CBSetAttr) (EI_API_CIP_NODE_T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, uint16_t len_p, void *pvValue_p) |
| Function prototype for CIP set attribute callback function. More...
|
|