EtherCAT Slave  1.04.06

◆ EC_API_SLV_EoE_CBSettingIndHandler_t

typedef bool(* EC_API_SLV_EoE_CBSettingIndHandler_t) (void *pContext_p, uint16_t *pMac_p, uint16_t *pIp_p, uint16_t *pSubNet_p, uint16_t *pDefaultGateway_p, uint16_t *pDnsIp_p)

EoE Settings Indication callback proxy.

Parameters
[in]pContext_pThe pointer to the EtherCAT API instance.
[in]pMac_pVirtual Net MAC address
[in]pIp_pVirtual Net IP address
[in]pSubNet_pVirtual Net Subnet
[in]pDefaultGateway_pVirtual Net Default Gateway
[in]pDnsIp_pVirtual Net DNS server address
Returns
true if settings are handled, false otherwise