![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
54 #ifndef MESSAGES_CORE_H
55 #define MESSAGES_CORE_H
TISCI_MSG_QUERY_MSMC request response providing currently available MSMC memory if present in the SoC...
Definition: tisci_core.h:281
Empty response for TISCI_MSG_BOARD_CONFIG_PM.
Definition: tisci_core.h:251
TISCI_MSG_VERSION request to provide version info about currently running firmware.
Definition: tisci_core.h:81
uint32_t tisci_boardcfg_rmp_high
Definition: tisci_core.h:129
uint8_t abi_major
Definition: tisci_core.h:85
uint32_t msmc_end_low
Definition: tisci_core.h:285
uint32_t tisci_boardcfg_pmp_low
Definition: tisci_core.h:237
TISCI_MSG_QUERY_MSMC request to provide currently available MSMC memory if present in the SoC.
Definition: tisci_core.h:265
uint32_t msmc_start_low
Definition: tisci_core.h:283
uint32_t tisci_boardcfgp_high
Definition: tisci_core.h:172
struct tisci_header hdr
Definition: tisci_core.h:155
uint32_t extboot_status
Definition: tisci_core.h:99
struct tisci_header hdr
Definition: tisci_core.h:282
Empty response for TISCI_MSG_BOARD_CONFIG_RESASG.
Definition: tisci_core.h:154
uint8_t abi_minor
Definition: tisci_core.h:86
struct tisci_header hdr
Definition: tisci_core.h:266
char str[32]
Definition: tisci_core.h:83
uint8_t patch_version
Definition: tisci_core.h:88
Empty response for TISCI_MSG_BOARD_CONFIG.
Definition: tisci_core.h:185
uint16_t version
Definition: tisci_core.h:84
struct tisci_header hdr
Definition: tisci_core.h:143
uint16_t tisci_boardcfg_security_size
Definition: tisci_core.h:206
TISCI_MSG_BOARD_CONFIG request to provide the location and size of the tisci_boardcfg structure.
Definition: tisci_core.h:169
struct tisci_header hdr
Definition: tisci_core.h:127
Empty response for TISCI_MSG_BOARD_CONFIG_SECURITY.
Definition: tisci_core.h:218
uint8_t devgrp_t
Defines the sysfw DEVGRP type. This is meant to be used in code or data structures that require disti...
Definition: sciclient.h:237
struct tisci_header hdr
Definition: tisci_core.h:186
uint16_t tisci_boardcfg_size
Definition: tisci_core.h:173
struct tisci_header hdr
Definition: tisci_core.h:111
uint32_t tisci_boardcfg_securityp_high
Definition: tisci_core.h:205
struct tisci_header hdr
Definition: tisci_core.h:82
Notification message to indicate the DMSC is available.
Definition: tisci_core.h:97
struct tisci_header hdr
Definition: tisci_core.h:252
uint32_t tisci_boardcfg_rmp_low
Definition: tisci_core.h:128
uint32_t tisci_boardcfg_pmp_high
Definition: tisci_core.h:238
struct tisci_header hdr
Definition: tisci_core.h:236
devgrp_t tisci_boardcfg_rm_devgrp
Definition: tisci_core.h:131
devgrp_t tisci_boardcfg_pm_devgrp
Definition: tisci_core.h:240
struct tisci_header hdr
Definition: tisci_core.h:219
TISCI_MSG_BOARD_CONFIG_RM request to provide the location and size of the tisci_boardcfg Resource Man...
Definition: tisci_core.h:126
Empty response for TISCI_MSG_BOARD_CONFIG_RM.
Definition: tisci_core.h:142
This file contains:
Definition: tisci_core.h:66
uint32_t tisci_boardcfg_securityp_low
Definition: tisci_core.h:204
Response to notification message about firmware availability.
Definition: tisci_core.h:110
uint16_t tisci_boardcfg_rm_size
Definition: tisci_core.h:130
struct tisci_header hdr
Definition: tisci_core.h:203
struct tisci_header hdr
Definition: tisci_core.h:170
uint32_t msmc_end_high
Definition: tisci_core.h:286
uint32_t tisci_boardcfgp_low
Definition: tisci_core.h:171
uint16_t tisci_boardcfg_pm_size
Definition: tisci_core.h:239
TISCI_MSG_BOARD_CONFIG_PM request to provide the location and size of the tisci_boardcfg Power Manage...
Definition: tisci_core.h:235
devgrp_t tisci_boardcfg_devgrp
Definition: tisci_core.h:174
struct tisci_msg_version_req __attribute__((__packed__))
struct tisci_header hdr
Definition: tisci_core.h:67
TISCI_MSG_BOARD_CONFIG_SECURITY request to provide the location and size of the tisci_boardcfg securi...
Definition: tisci_core.h:202
uint8_t sub_version
Definition: tisci_core.h:87
devgrp_t tisci_boardcfg_security_devgrp
Definition: tisci_core.h:207
struct tisci_header hdr
Definition: tisci_core.h:98
uint32_t msmc_start_high
Definition: tisci_core.h:284