![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
57 #define SOC_DOMAIN_ID_MAIN (0U)
58 #define SOC_DOMAIN_ID_MCU (1U)
64 #define SOC_BOOTMODE_MMCSD (0X36C3)
This file contains prototypes for APIs contained as a part of SCICLIENT as well as the structures of ...
int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
Set module clock to specified frequency.
void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition)
Unlock control module partition to allow writes into control MMRs.
uint64_t SOC_virtToPhy(void *virtAddr)
SOC Virtual (CPU) to Physical address translation function.
int32_t SOC_moduleGetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)
Get module clock frequency.
void * SOC_phyToVirt(uint64_t phyAddr)
Physical to Virtual (CPU) address translation function.
uint64_t SOC_getSelfCpuClk(void)
Get the clock frequency in Hz of the CPU on which the driver is running.
void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition)
Lock control module partition to prevent writes into control MMRs.
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable)
Enable clock to specified module.
void SOC_setDevStat(uint32_t bootMode)
Change boot mode by setting devstat register.
const char * SOC_getCoreName(uint16_t coreId)
Convert a core ID to a user readable name.
void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable)
Enable or disable ePWM time base clock from Control MMR.
@ enable
Definition: iPtcpDrv.h:63