PROFINET Device  v1.04.02

◆ PN_API_DEV_getBufferOutputData()

uint32_t PN_API_DEV_getBufferOutputData ( uint8_t **  ppBuffer_p)

Get buffer of output data triple buffer of IO device with last written output data.

ToDo.

Parameters
[out]ppBuffer_pBuffer with last written output data.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run