EtherNet/IP™ Adapter  1.04.00
User Reference Manual

◆ EI_API_ADP_getQuickConnectEnabled()

uint32_t EI_API_ADP_getQuickConnectEnabled ( T *  pAdp_p,
bool *  pQuickConnectEnabled_p 
)

Get the current adapter QuickConnect state (Instance Attribute ID: 12).

Function that returns the adapter QuickConnect state.

Value Description
0 Disabled
1 Enabled
Parameters
[in]pAdp_pPointer to the adapter.
[out]pQuickConnectEnabled_pPointer of type uint8_t to the adapter QuickConnect state.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t quickConnectEnabled;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getQuickConnect(pEI_API_ADP, &quickConnectEnabled);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:232
See also
EI_API_ADP_setQuickConnectEnabled EI_API_ADP_EError_t