|
AM64x MCU+ SDK
08.01.00
|
|
Go to the documentation of this file.
33 #ifndef ICSS_EIP_MCFLTR_H_
34 #define ICSS_EIP_MCFLTR_H_
void eip_multicast_filter_init(PRUICSS_Handle pruicssHandle)
multicast filtering init
void eip_multicast_filter_config(PRUICSS_Handle pruicssHandle, uint8_t command)
configuration to enable/disable multicast filtering
void eip_multicast_filter_override_hashmask(PRUICSS_Handle pruicssHandle, char *mask)
configure the mask
void eip_multicast_filter_update_macid(PRUICSS_Handle pruicssHandle, char *multicastAddr, uint8_t command)
insert/delete a multicast MAC ID in the multicast filter table
void eip_multicast_stromPrev_config(PRUICSS_Handle pruicssHandle, uint8_t command)
configuration to enable/disable storm prevention for multicast traffic
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/g_v0/pruicss.h:234