AM64x MCU+ SDK  08.01.00
Crypto AES

Advanced Encryption Standard (AES) is widely adopted symmetric Encrypt/Decrypt algorithm provides information security such as confidentiality ..

Features Supported

  • Supports Aes_cbc_256, Aes_cbc_128 and Aes_cbc_192 operations
  • Supports Aes_cmac_256, Aes_cmac_128 and Aes_cmac_192 operations
  • Encryption and Decryption
  • Symmetric key symmetric block cipher

SysConfig Features

Features NOT Supported

Usage Overview

AES Cipher Block Chaining (CBC) API Sequence

To use the AES driver to do Encryption and decryption. Use the following APIs:

AES Cipher-based Message Authentication Code (CMAC) API Sequence

To use the AES driver to do CMAC. Use the following APIs:

  • Crypto_AesParams_init() : Call this API to set defaults and then override the fields as needed before calling Crypto_aesOpen.
  • Crypto_aesOpen() : Initializes a AES context and gives the configuration based on instance.
  • Crypto_cmacSingleShot() : This function calculates the Advance Encryption Standard Cipher-based Message Authentication Code (AES-CMAC) of a buffer.
  • Crypto_cmacSetup() : This function prepares a cipher context for use with the given cipher primitive.
  • Crypto_cmacStarts() : This function sets the CMAC key, and prepares to authenticate the input data.
  • Crypto_cmacUpdate() : This function feeds an input buffer into an ongoing CMAC computation.
  • Crypto_cmacFinish() : This function finishes the CMAC operation, and writes the result to the output buffer.
  • Crypto_aesClose() : De-initialize the AES instance and Clears AES context.

Initializing the AES Driver context buffer

  • Crypto_aesOpen() must be called before any other AES APIs. This function Initializes a AES context and iterates through the elements of the gCryptoAesConfig[] array. Please note that initializing AES driver is taken care by the SysConfig generated code.

AES_CBC Encryption and Decryption

Generating AES_CMAC

Clearing the AES Driver context buffer

Important Usage Guidelines

Example Usage

Include the below file to access the APIs

#include <stdio.h>
#include <string.h>
#define APP_AES_OUTPUT_LENGTH (16)
uint8_t gCryptoAesTestBuf[16]={0x81,0xEA,0x5B,0xA4,0x69,0x45,0xC1,0x70,0x5F,0x6F,0x89,0x77,0x88,0x68,0xCC,0x67};
uint8_t gCryptoAesTestKey[32]={0x33,0xA3,0x66,0x46,0xFE,0x56,0xF7,0x0D,0xC0,0xC5,0x1A,0x31,0x17,0xE6,0x39,0xF1,0x82,0xDE,0xF8,0xCA,0xB5,0xC0,0x66,0x71,0xEE,0xA0,0x40,0x7C,0x48,0xA9,0xC7,0x57};
uint8_t gCryptoAesTestIv[16]={0x7C,0xE2,0xAB,0xAF,0x8B,0xEF,0x23,0xC4,0x81,0x6D,0xC8,0xCE,0x84,0x20,0x48,0xA7};

Aes cbc Example

Crypto_AesHandle aesHandle;
uint8_t aesResultBuf[APP_AES_OUTPUT_LENGTH];
int32_t status;
/* Context memory */
static Crypto_AesContext gCryptoAesContext;
/* Aes encryption */
memcpy(&params.iv, gCryptoAesTestIv, CRYPTO_AES_IV_LENGTH);
memcpy(&params.key, gCryptoAesTestKey, CRYPTO_AES_KEY_LENGTH);
params.keySizeInBits = 256;
params.type = CRYPTO_TYPE_SW;
aesHandle = Crypto_aesOpen(&gCryptoAesContext, &params);
status = Crypto_aesSetKeyEnc(aesHandle);
status = Crypto_aesCbc(aesHandle, gCryptoAesTestBuf, sizeof(gCryptoAesTestBuf), aesResultBuf );
status = Crypto_aesClose(aesHandle);
/* Aes Decryption */
memcpy(&params.iv, gCryptoAesTestIv, CRYPTO_AES_IV_LENGTH);
memcpy(&params.key, gCryptoAesTestKey, CRYPTO_AES_KEY_LENGTH);
params.keySizeInBits = 256;
params.type = CRYPTO_TYPE_SW;
aesHandle = Crypto_aesOpen(&gCryptoAesContext, &params);
status = Crypto_aesSetKeyDec(aesHandle);
status = Crypto_aesCbc(aesHandle, gCryptoAesTestBuf, sizeof(gCryptoAesTestBuf), aesResultBuf );
status = Crypto_aesClose(aesHandle);

API

APIs for CRYPTO AES

CRYPTO_AES_IV_LENGTH
#define CRYPTO_AES_IV_LENGTH
IV buffer length should be 16 bytes.
Definition: crypto_aes.h:92
Crypto_aesSetKeyEnc
int32_t Crypto_aesSetKeyEnc(Crypto_AesHandle handle)
This function sets the Advance Encryption Standard (AES) encryption key.
Crypto_AesParams::algoType
uint32_t algoType
Definition: crypto_aes.h:114
Crypto_AesParams::key
uint8_t key[CRYPTO_AES_KEY_LENGTH]
Definition: crypto_aes.h:118
Crypto_AesParams::type
uint32_t type
Definition: crypto_aes.h:122
Crypto_AesParams::iv
uint8_t iv[CRYPTO_AES_IV_LENGTH]
Definition: crypto_aes.h:116
Crypto_aesCbc
int32_t Crypto_aesCbc(Crypto_AesHandle handle, const uint8_t *input, uint32_t ilen, uint8_t *output)
This function finishes the Advance Encryption Standard Cipher Block Chaining (AES-CBC) operation,...
Crypto_aesOpen
Crypto_AesHandle Crypto_aesOpen(Crypto_AesContext *ctx, const Crypto_AesParams *params)
This function gives the configuration based on type.
CRYPTO_AES_ENCRYPT
#define CRYPTO_AES_ENCRYPT
AES encryption algorithm.
Definition: crypto_aes.h:67
Crypto_AesHandle
void * Crypto_AesHandle
Handle to the Crypto AES driver returned by Crypto_aesOpen()
Definition: crypto_aes.h:98
Crypto_AesParams
Parameters passed during Crypto_aesOpen()
Definition: crypto_aes.h:111
Crypto_aesClose
int32_t Crypto_aesClose(Crypto_AesHandle handle)
This function clears a Advance Encryption Standard (AES) context.
CRYPTO_AES_DECRYPT
#define CRYPTO_AES_DECRYPT
AES decryption algorithm.
Definition: crypto_aes.h:65
Crypto_aesSetKeyDec
int32_t Crypto_aesSetKeyDec(Crypto_AesHandle handle)
This function sets the Advance Encryption Standard (AES) decryption key.
Crypto_AesParams::keySizeInBits
uint32_t keySizeInBits
Definition: crypto_aes.h:120
crypto_aes.h
CRYPTO_AES_KEY_LENGTH
#define CRYPTO_AES_KEY_LENGTH
key buffer length, min 16 bytes and max 32 bytes
Definition: crypto_aes.h:95