AM64x MCU+ SDK  08.01.00
Release Notes 07.03.02

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
All SW modules will not work on M4F. M4F support for a module will be explicitly called out.

New in this Release

Feature Module
FreeRTOS APIs for event group DPL
DebugP_log to memory and view in ROV DPL
TinyUSB stack with CDC USB
DDR driver support DDR
eQEP driver support eQEP
eCAP driver support eCAP
IPC RPMessage RX notify callback IPC RPMessage
MCSPI Read RX data low-overhead API McSPI
Generic NOR Flash APIs for 1s1s1s mode as part of OSPI driver OSPI

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM64x R5F, M4F AM64x GP EVM (referred to as am64x-evm in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F, M4F 11.0.0
SysConfig R5F, M4F 1.10.0, build 2163
TI ARM CLANG R5F, M4F 1.3.0.LTS
FreeRTOS Kernel R5F, M4F 10.4.3

Key Features

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F, M4F NA Task, Task notification, interrupts, semaphores, mutexs, timers. ROV views in CCS IDE Task load measurement using FreeRTOS run time statistics APIs.
FreeRTOS POSIX R5F, M4F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F, M4F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Address Translate M4F YES FreeRTOS, NORTOS Use RAT to allow M4F access to peripheral address space -
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F, M4F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CycleCounter R5F, M4F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F, M4F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F, M4F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F, M4F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F, M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F, M4F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F, M4F NA FreeRTOS Create, delete tasks -
Timer R5F, M4F YES FreeRTOS, NORTOS Configure arbitrary timers -
Event R5F, M4F YES FreeRTOS Setting, getting, clearing, and waiting of Event bits -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, OSPI XIP, UART. All R5F's, M4F boot. RPRC, multi-core image format, DDR init SBL booting Linux. SBL booting A53.

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
ADC R5F YES Single conversion (one-shot mode), interrupt mode, DMA mode Continuous conversion not tested
CRC R5F NO Only compiled Not tested
DDR R5F YES Tested LPDDR4 at 400MHz frequency. -
ECAP R5F YES Frequency, Duty cycle, interrupt mode PWM mode not tested
EPWM R5F YES Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module Tripzone module not tested
EQEP R5F YES Signal Frequency and Direction, interrupt mode -
FSI (RX/TX) R5F YES RX, TX, polling, interrupt mode, single/dual lanes -
GPIO R5F, M4F YES Basic input/output, GPIO as interrupt -
I2C R5F, M4F YES Master mode, basic read/write, polling and interrupt mode Slave mode not supported. M4F not tested due to EVM limitation
IPC Notify R5F, M4F YES Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F YES RPMessage protocol based IPC, All R5F and Linux A53 cores M4F core not supported
MCAN R5F YES RX, TX, interrupt and polling mode -
MCSPI R5F, M4F YES Master/Slave mode, basic read/write, polling, interrupt mode DMA mode not supported
MDIO R5F NA Register read/write, link status and link interrupt enable API -
OSPI R5F YES Read direct, Write indirect, Read/Write commands, DMA for read, PHY Mode Interrupt mode not supported
Pinmux R5F, M4F YES Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES Tested with Ethercat FW HAL, HDSL, EnDat More protocols integration tests pending
SOC R5F, M4F YES lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency -
Sciclient R5F, M4F YES Tested with clock setup, module on/off -
SPINLOCK R5F, M4F NA Lock, unlock HW spinlocks -
UART R5F, M4F YES Basic read/write, polling, interrupt mode, HW flow control not tested. DMA mode not supported
UDMA R5F YES Basic memory copy, SW trigger, Chaining -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES I2C based EEPROM -
ETHPHY R5F YES Ethernet Phy configuration for EtherCAT Slave example -
Flash R5F YES XSPI, OSPI, QSPI based flash, Octal, Quad mode, DDR mode All vendor flash types not tested
LED R5F YES GPIO and I2C IO expander based LED control -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
CMSIS DSP R5F NA FreeRTOS, NORTOS Basic math, complex math, controller, fast math, filtering, Matrix, statistics, transform -

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Position Sense HDSL R5F YES FreeRTOS, NORTOS Freerun mode, Sync mode -
Position Sense EnDAT R5F YES FreeRTOS, NORTOS Single channel, Multi channel, Continuous mode -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT Slave FW HAL R5F YES FreeRTOS Tested with Beckhoff's EtherCAT stack based example Online firmware update, reset isolation
EtherCAT Slave ETG Stack R5F NO FreeRTOS Standard stack (NOT BUNDLED in SDK) -
EtherNet/IP Adapter FW HAL R5F NO FreeRTOS Only compiled Not tested
Profinet Device FW HAL R5F NO FreeRTOS Only compiled Not tested
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested
ICSS TimeSync R5F NO FreeRTOS Only compiled Not tested

USB

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
USB SoC Porting Layer R5F YES FreeRTOS, NORTOS USB 2.0 device mode USB 3.0
USB Device Driver R5F NO FreeRTOS, NORTOS USB 2.0 device mode USB Host driver
TinyUSB Core and CDC Driver R5F NO FreeRTOS, NORTOS USB device with CDC class USB Host, other USB device class drivers

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Benchmark demo 4xR5F's YES NORTOS CFFT, FIR and FOC benchmarks ADC/PWM benchmark

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-596 Zero init of globals and static does not happen with current compiler and linker option Common 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-627 Bootloader: R5FSS0_0 ATCM is not enabled after NULL SBL boot Bootloader 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-675 XIP: OSPI @ 166Mhz with Phy enable and Phy pipeline enable and XIP does not work Bootloader, XIP 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-648 DLFO bit is set unconditionally during CacheP_init() for R5 Core DPL 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-177 DMTimer on M4F results in 2 interrupts instead of 1 for every DM timer expiry in release mode DPL 7.3.0 AM64x, AM243x Fixed
MCUSDK-795 ClockP_usleep sleeps for more than the value passed DPL 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-316 ROV does not work with DDR being used in application ROV 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-354 EtherCAT State Machine from EtherCAT Conformance Test fails intermittently EtherCAT 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-686 Incorrect MAC is compared for processing PTP frames in EIP_processProtocolFrames EtherNet/IP Adapter FW HAL 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-796 bsp_pdi_write_indication not called after writing EEPROM Control/Status register write in bsp_init EtherCAT Slave FW HAL 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-757 Incorrect pin calculation in SysConfig generated code for I2C IO expander LED 7.3.0, 7.3.1 AM64x, AM243x Fixed
MCUSDK-781 SysConfig for multiple GPIO LED instances generate same code LED 7.3.0, 7.3.1 AM64x, AM243x Fixed

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
MCUSDK-317 OSPI: DMA reads fails after a flash write which was not block aligned OSPI 7.3.0 onwards AM64x, AM243x Use non-DMA read mode or use DMA mode but always write from start of a erased block
MCUSDK-683 UDMA: DMA from SRAM to M4F IRAM/DRAM fails UDMA, TIFS 7.3.0 onwards AM64x, AM243x Don't use these memories for DMA transfer or perform manual copy
MCUSDK-867 Rx is not selected in the pins for EtherCAT and Ethernet pinmux from SysConfig EtherCAT Slave FW HAL, ICSS-EMAC 7.3.0 onwards AM64x, AM243x Rx checkbox should to be selected manually
MCUSDK-750 ICSS PRU GPIO pins are not supported by SYSCFG SysCfg 7.3.0 onwards AM64x, AM243x Perform manual pinmux
MCUSDK-906 MCAN and ADC not functional in SBL UART bootmode with DDR enabled Bootloader, DDR 7.3.2 AM64x, AM243x Explicitly enable DDR in the application instead of SBL UART.
MCUSDK-892 USB boot with SBL OSPI fails USB 7.3.2 AM64x, AM243x Use UART boot or CCS loading
MCUSDK-626 DMA not working with ADC FIFO 1 ADC 7.3.0 onwards AM64x, AM243x Use ADC FIFO 0

Limitations

ID Head Line Module Reported in Release Applicable Devices Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 7.3.0 AM64x, AM243x Use bash for windows as part of git for windows or don't use -j option

Upgrade and Compatibility Information

Attention
When migrating from Processor SDK RTOS, see Migration Guides for more details

Examples

Module Affected API Change Additional Remarks
All examples Linker command file

To enable support for zero init of uninitialized globals in .bss section an update in linker command file is needed. Add below in your project linker.cmd file if not already there.

...
.bss: {} palign(8) /* This is where uninitialized globals go */
RUN_START(__BSS_START) /* ADD THIS LINE after the .bss line */
RUN_END(__BSS_END) /* AND THIS LINE as well */
...

All SDK examples are updated for this change. This change is needed in your application if it based off a older SDK.

Networking

Module Affected API Change Additional Remarks
EtherCAT Slave FWHAL bsp_init Added new parameter enhancedlink_enable in bsp_params Provides flexibility to enable/disable enhanced link detection.
EtherNet/IP Adapter FW HAL - Added new parameter macId in EIP_DLRHandle structure This field should be filled by the user before calling EIP_drvInit
EtherNet/IP Adapter FW HAL - cipSyncConfig_t structure inside eip_Config structure is allocated statically -
ICSS-EMAC - Added phyToMacInterfaceMod and txInterruptEnable in ICSS_EMAC_Attrs ICSS configuration is done for MII/RGMII based on the mode selected using phyToMacInterfaceMode. Task and interrupt for TX will be created only if txInterruptEnable is enabled.
ICSS-EMAC ICSS_EMAC_Params_init Moved macId from ICSS_EMAC_Attrs to ICSS_EMAC_Params It provides flexibility to provide the mac address during run-time.
ICSS TimeSync - Added new parameter macId in TimeSync_ParamsHandle structure This field should be filled by the user.

SOC Device Drivers

Module Affected API Change Additional Remarks
OSPI - Removed parameters pageSize and blkSize from OSPI_Attrs structure and added new API OSPI_setDeviceSize to set this. This has to be called in respective flash driver's open to set this. The parameters can't be assumed at the time of OSPI driver open, so this has to be set with the OSPI_setDeviceSize API. If not using OSPI APIs directly, this change can be ignored. This is already taken care in the provided flash drivers.
OSPI - Removed fields rdDummyClks and extRdDummyClks from OSPI_Attrs and rdStatusCmd from OSPI_Object as these are not used anymore -
OSPI - Added support to set which type of command extension to be used in case of flashes with Octal DDR support. Can use the OSPI_setCmdExtType API in the respective flash driver's open to set this. If not using OSPI APIs directly, this change can be ignored. This is already taken care in the provided flash drivers.
OSPI Internal APIs in respective flash drivers were changed. Revamped the OSPI_ReadCmdParams and OSPI_WriteCmdParams structure to separate cmd and address. Also added a new field numAddrBytes. If not using OSPI APIs directly, this change can be ignored. This is already taken care in the provided flash drivers.
OSPI - Added new fields rdDataCapDelay, phyRdDataCapDelay, numAddrBytes and cmdExtType to OSPI_Object for book keeping. These will be filled in the flash driver using APIs OSPI_setRdDataCaptureDelay, OSPI_setNumAddrBytes and OSPI_setCmdExtType. The phyRdDataCapDelay variable will be updated by the PHY tuning algorithm
OSPI OSPI_setXferOpcode OSPI_setXferOpcode API is changed to OSPI_setXferOpCodes. The parameter readStatusCmd has been removed from this API since it is no longer needed

-