AM64x MCU+ SDK  08.01.00
OSPI Migration Guide

This section describes the differences between OSPI APIs of MCU+ SDK and Processor SDK RTOS (PDK). This can be used as a migration aid when moving from Processor SDK RTOS (PDK) to MCU+ SDK.

In MCU+ SDK, the OSPI module provides higher level driver APIs.Refer OSPI for more details. From the user point of view, higher level API usage is same as in PDK.APIs name begins with OSPI_ instead of SPI_.

API changes

There are changes in API names, structure names and macro names. The changes in function names are listed below.

PDK MCU+ SDK Remarks
SPI_init OSPI_init API rename
None OSPI_deinit In MCU+SDK, this API can be used to de-initializes the OSPI module
SPI_open OSPI_open API rename
SPI_Params_init OSPI_Params_init API rename
SPI_close OSPI_close API rename
SPI_close OSPI_close API rename
SPI_serviceISR None In MCU+SDK, ISR is handled inside the driver.
SPI_transfer None In MCU+SDK, SPI_transfer is separated into sub APIs OSPI_readDirect, OSPI_writeDirect, OSPI_readIndirect, OSPI_writeIndirect
SPI_transferCancel None In MCU+SDK, API is not supported.
SPI_control None In MCU+SDK, SPI_control is separated into sub APIs OSPI_readCmd, OSPI_writeCmd, OSPI_enableDdrRdCmds and so on. API are listed below.
None OSPI_getHandle In MCU+SDK, this API can be used to return the handle of an open OSPI Instance from the instance index
None OSPI_readDirect In MCU+SDK, this API can be used to perform direct reads from the flash using DAC controller
None OSPI_readIndirect In MCU+SDK, this API can be used to perform indirect reads from the flash using INDAC controller
None OSPI_writeDirect In MCU+SDK, this API can be used to perform direct writes to the flash using DAC controller
None OSPI_writeIndirect In MCU+SDK, this API can be used to perform indirect writes to the flash using INDAC controller
None OSPI_readCmd In MCU+SDK, this API can be used to send specific commands and receive related data from flash
None OSPI_writeCmd In MCU+SDK, this API can be used to send specific commands and related data to flash
None OSPI_Transaction_init In MCU+SDK, this API can be used to initialize the OSPI_Transaction structure
None OSPI_ReadCmdParams_init In MCU+SDK, this API can be used to initialize the OSPI_ReadCmdParams structure
None OSPI_WriteCmdParams_init In MCU+SDK, this API can be used to initialize the OSPI_WriteCmdParams structure
None OSPI_isDacEnable In MCU+SDK, this API can be used to check if the Direct Access Controller is enabled
None OSPI_isDmaEnable In MCU+SDK, this API can be used to check if DMA is enabled for reads
None OSPI_isIntrEnable In MCU+SDK, this API can be used to check if interrupts are enabled
None OSPI_isPhyEnable In MCU+SDK, this API can be used to check if the OSPI PHY controller is enabled
None OSPI_isDtrEnable In MCU+SDK, this API can be used to check if the Dual Transfer Rate is enabled
None OSPI_enableDDR In MCU+SDK, this API can be used to enable the Dual Data Rate (DDR)
None OSPI_enableSDR In MCU+SDK, this API can be used to enable the Single Data Rate (SDR)
None OSPI_enableDdrRdCmds In MCU+SDK, this API can be used to set DDR bit in INSTR_RD register for RD commands
None OSPI_setRdDataCaptureDelay In MCU+SDK, this API can be used to set read data capture cycles in the OSPI controller
None OSPI_setNumAddrBytes In MCU+SDK, this API can be used to set the number of bytes used to send address while reading or writing to flash memory
None OSPI_setDeviceSize In MCU+SDK, this API can be used to set the block size and page size of the flash to the device size register in OSPI
None OSPI_setCmdDummyCycles In MCU+SDK, this API can be used to set appropriate dummy cycles to be used while sending STIG commands to flash
None OSPI_setReadDummyCycles In MCU+SDK, this API can be used to set appropriate dummy cycles for flash read
None OSPI_setPhyEnableSuccess In MCU+SDK, this API can be used to set the phyEnableSuccess field in OSPI_Object. Has to be called from flash driver
None OSPI_getPhyEnableSuccess In MCU+SDK, this API can be used to fetch the phyEnableSuccess field in OSPI_Object.
None OSPI_cmdModeBitSet In MCU+SDK, this API can be used to set command mode bit
None OSPI_rdModeBitSet In MCU+SDK, this API can be used to set Read mode bit
None OSPI_setXferLines In MCU+SDK, this API can be used to set the number of transfer lines to the OSPI controller
None OSPI_getXferLines In MCU+SDK, this API can be used to return the current number of transfer lines set in the OSPI controller
None OSPI_setDualOpCodeMode In MCU+SDK, this API can be used to set OSPI controller to use dual byte opcodes
None OSPI_setXferOpCodes In MCU+SDK, this API can be used to set the opcodes for reading and page programming the flash
None OSPI_setCmdExtType In MCU+SDK, this API can be used to set the type of command extension used in dual byte opcode mode
None OSPI_enableDacMode In MCU+SDK, this API can be used to enable the Direct Access Mode
None OSPI_disableDacMode In MCU+SDK, this API can be used to disable the Direct Access Mode
None OSPI_getFlashDataBaseAddr In MCU+SDK, this API can be used to get the SOC mapped data base address of the flash
None OSPI_phyTuneDDR In MCU+SDK, this API can be used to tune the OSPI PHY for DDR mode to set optimal PHY parameters
None OSPI_phyTuneGrapher In MCU+SDK, this API takes a 4x128x128 array and fills it with TX RX DLL data for graphing purpose
None OSPI_phyGetTuningData In MCU+SDK, this API can be used to return the address to the attack vector buf required for tuning the PHY
None OSPI_phyReadAttackVector In MCU+SDK, this API can be used to check if the attack vector, or the data used for tuning the PHY is present at an offset in the flash
None OSPI_enablePhy In MCU+SDK, this API can be used to enable the PHY
None OSPI_disablePhy In MCU+SDK, this API can be used to disable the PHY
None OSPI_enablePhyPipeline In MCU+SDK, this API can be used to enable the PHY Pipeline
None OSPI_disablePhyPipeline In MCU+SDK, this API can be used to disable the PHY Pipeline
None OSPI_norFlashInit1s1s1s In MCU+SDK, this API can be used to initialize the NOR flash to work in 1-1-1 mode
None OSPI_norFlashReadId In MCU+SDK, this API can be used to read the JEDEC ID from the NOR flash connected to the OSPI peripheral
None OSPI_norFlashWrite In MCU+SDK, this API can be used to write data to the flash at a specified offset
None OSPI_norFlashRead In MCU+SDK, this API can be used to read data from the flash from a specified offset
None OSPI_norFlashReadSfdp In MCU+SDK, this API can be used to read SFDP table from the flash from a specified offset
None OSPI_norFlashErase In MCU+SDK, this API can be used to erase 1 block of data starting from a provided address

Important Notes

  • In MCU+ SDK, Users are recommended to use SysConfig as this will greatly simplify the task of driver configuration.

See Also