AM64x MCU+ SDK  08.01.00
GPIO Migration Guide

This section describes the differences between GPIO APIs of MCU+ SDK and Processor SDK RTOS (PDK). This can be used as a migration aid when moving from Processor SDK RTOS (PDK) to MCU+ SDK.

In MCU+ SDK, the GPIO APIs are simplified. Most of the CSL and LLD are merged into single API. Refer GPIO for more details.

API changes

There are changes in functions names, structure names and macro names. The changes in function names are listed below.

PDK MCU+ SDK Change Description / Remarks
GPIO_setConfig GPIO_setDirMode In MCU+SDK, this GPIO_setConfig is separated into sub APIs such as GPIO_setTrigType, GPIO_setDirMode.
GPIO_write GPIO_pinWriteHigh API rename along with interface parameter changes.
GPIO_write GPIO_pinWriteLow API rename along with interface parameter changes.
GPIO_read GPIO_pinRead API rename along with interface parameter changes.
None GPIO_pinOutValueRead In MCU+SDK, this API can be used to determine the output logic level(value) on a specified GPIO pin.
GPIO_setConfig GPIO_setTrigType In MCU+SDK, this GPIO_setConfig is separated into sub APIs such as GPIO_setTrigType, GPIO_setDirMode.
None GPIO_bankIntrEnable In MCU+SDK, this API can be used to enable the bank interrupt.
None GPIO_bankIntrDisable In MCU+SDK, this API can be used to disable the bank interrupt.
None GPIO_getIntrStatus In MCU+SDK, this API can be used to determine the enabled interrupt status of a specified pin.
GPIO_clearInt GPIO_clearIntrStatus In MCU+SDK, this API can be used to clear the enabled interrupt status of a specified pin.
None GPIO_getBankIntrStatus In MCU+SDK, this API is used to return the interrupt status of the specified bank.
None GPIO_clearBankIntrStatus In MCU+SDK, this API is used to clear the interrupt status of the specified bank.
GPIO_disableInt None In MCU+SDK, Bank interrupt disable is available instead of specific pin.
GPIO_enableInt None In MCU+SDK, Bank interrupt enable is available instead of specific pin.
GPIO_init None Removed as abstraction is done with simplified APIs.
GPIO_setCallback None Not Applicable.
GPIO_toggle None None

Important Notes

  • In MCU+ SDK, users are recommended to use SysConfig as this will greatly simplify the task of driver configuration.

See Also