AM64x MCU+ SDK  08.01.00
Sciclient Get Version

Introduction

This example demonstrates how to check the version of SYSFW running on the Cortex M3 at run time. Since this is frequently done by bootloaders as a sanity check, there is an API included in the Sciclient driver for checking the SYSFW version.

However, in this example this API is not used, instead the basic Sciclient_service API is used to send a "GET VERSION" request to the SYSFW and get a response back and print it out.

We also fetch the clock frequency of the current CPU using Sciclient and print that out as well, as additional sanity check.

Supported Combinations

Attention
A53 NORTOS support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-1 nortos
r5fss1-0 nortos
r5fss1-1 nortos
m4fss0-0 nortos
a53ss0-0 nortos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm
Example folder examples/drivers/sciclient/sciclient_get_version

Steps to Run the Example

See Also

SCICLIENT

Sample Output

Shown below is a sample output when the application is run,

DMSC Firmware Version 21.1.1--v2021.01a (Terrific Lla
Firmware revision 0x15
ABI revision 3.1
[SCICLIENT] CPU clock frequency = 800000000 Hz
All tests have passed!!