Introduction
This example demonstrates the how to generate SHA hash.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am64x-evm |
Example folder | examples/security/crypto/crypto_sha_sw/crypto_sha_sw.c |
Steps to Run the Example
See Also
SA2UL
Sample Output
Shown below is a sample output when the application is run.
CCS Console:
[CRYPTO] SHA HW example started ...
[CRYPTO] Data length : 9 bytes
[CRYPTO] Total ticks : 30514
[CRYPTO] Total throughput In MBps : 0.235957
[CRYPTO] SHA-512 HW example completed!!
[CRYPTO] Data length : 9 bytes
[CRYPTO] Total ticks : 23976
[CRYPTO] Total throughput In MBps : 0.300300
[CRYPTO] SHA-256 HW example completed!!
All tests have passed!!