AM64x MCU+ SDK  08.01.00
SPINLOCK

The Spinlock driver provides API to program the Spinlock module to synchronize processes running on multiple processors in the device.

Features Supported

  • 256 spinlocks
  • Lock and unlock API

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • Not applicable/supported

Features NOT Supported

NA

Important Usage Guidelines

  • The Spinlock driver doesn't enforce below limitation as defined in device manual. It is the responsibility of the application to take care of below recommendations
  • Spinlock is appropriate for mutual exclusion for access to a shared data structure. It should be used only when:
    • The time to hold the lock is predictable and small (for example, a maximum hold time of less than 200 CPU cycles may be acceptable).
    • The locking task cannot be preempted, suspended, or interrupted while holding the lock (this would make the hold time large and unpredictable).
    • The lock is lightly contended, that is the chance of any other process (or processor) trying to acquire the lock while it is held is small.

Example Usage

Include the below file to access the APIs

Lock API

int32_t status;
/* Spin till lock is acquired */
while(1U)
{
status = Spinlock_lock(spinlockBaseAddr, lockNum);
{
break; /* Free and taken */
}
}
/*
* enter critical section
*/

Unlock API

Spinlock_unlock(spinlockBaseAddr, lockNum);

API

APIs for SPINLOCK

spinlock.h
Spinlock_lock
int32_t Spinlock_lock(uint32_t baseAddr, uint32_t lockNumber)
This API performs the Read operation for Lock status of the SPINLOCK_LOCK_REG, in order to acquire a ...
Spinlock_unlock
void Spinlock_unlock(uint32_t baseAddr, uint32_t lockNumber)
This API performs the write operation for Lock status of the SPINLOCK_LOCK_REG, in order to Free the ...
SPINLOCK_LOCK_STATUS_FREE
#define SPINLOCK_LOCK_STATUS_FREE
Flag to indicate spinlock is free.
Definition: spinlock/v0/spinlock.h:69