PROFINET Device  v1.04.01

◆ PN_API_DEV_registerConnectResponseCallback()

uint32_t PN_API_DEV_registerConnectResponseCallback ( PN_API_DEV_connectResponseCallback  cbFunction_p)

Register IO device callback indicating a connect response is to be sent on application relation establishment.

ToDo.

Parameters
[in]cbFunction_pCallback function.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run