PROFINET Device  v1.04.01

◆ PN_API_DEV_registerReadRecordIndicatedCallback()

uint32_t PN_API_DEV_registerReadRecordIndicatedCallback ( PN_API_DEV_readRecordIndicatedCallback  cbFunction_p)

Register IO device callback indicating a read record request has been received.

ToDo.

Parameters
[in]cbFunction_pCallback function.
Returns
PN_API_DEV_EError_t as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start PN_API_PDEV_run