PROFINET Device
v1.04.01
◆
PN_API_DEV_setApplicationReady()
uint32_t PN_API_DEV_setApplicationReady
(
PN_API_DEV_EAr_t
ar_p
)
Set IO device application ready on application relation establishment.
ToDo.
Parameters
[in]
ar_p
Application relation.
Returns
PN_API_DEV_EError_t
as uint32_t
Return values
PN_API_DEV_eOK
Example
#include <PN_API_DEV.h>
See also
PN_API_PDEV_start
PN_API_PDEV_run
PROFINET Device API
generated by
1.8.18