EtherCAT Slave  1.04.05

◆ EC_SLV_APP_EoE_settingIndHandler()

bool EC_SLV_APP_EoE_settingIndHandler ( void *  pContext_p,
uint16_t *  pMac_p,
uint16_t *  pIp_p,
uint16_t *  pSubNet_p,
uint16_t *  pDefaultGateway_p,
uint16_t *  pDnsIp_p 
)

EoE Settings Indication callback.

Parameters
[in]pContext_pThe pointer to the application instance.
[in]pMac_pVirtual Net MAC address
[in]pIp_pVirtual Net IP address
[in]pSubNet_pVirtual Net Subnet
[in]pDefaultGateway_pVirtual Net Default Gateway
[in]pDnsIp_pVirtual Net DNS server address
Returns
true if settings are handled, false otherwise