EtherCAT Slave  1.04.05

◆ EC_API_SLV_FoE_CBReadFileHandler_t

typedef uint32_t(* EC_API_SLV_FoE_CBReadFileHandler_t) (void *pContext_p, uint16_t *pData_p, uint16_t foeMaxSendBlockSize_p, uint32_t offset_p)

Read FoE File callback.

Parameters
[in]pContext_pcall context
[in]pData_pFoE file data
[in]foeMaxSendBlockSize_pMax SendBlock Size
[in]offset_pFoE file data offset
Returns
Error Code.