Introduction
This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.
Supported Combinations
- Attention
- A53 NORTOS support is experimental and is NOT supported by TI.
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
m4fss0-0 nortos |
a53ss0-0 nortos |
Toolchain | ti-arm-clang |
arm.gnu.aarch64-none |
Board | am64x-evm |
Example folder | examples/drivers/gpio/gpio_led_blink/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Watch out for LED LD26 on the EVM to blink which is controlled by MCU_GPIO0_5.
See Also
GPIO
Sample Output
Shown below is a sample output when the application is run,
GPIO LED Blink Test Started ...
LED will Blink for 10 seconds ...
GPIO LED Blink Test Passed!!
All tests have passed!!