A description of an externally visible characteristic or feature of an object. Attributes may provide status information or govern the operation of an object. For example: the ASCII name of an object, the repetition rate of a cyclic object.
Functions | |
uint32_t | EI_API_CIP_setAttr_bool (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_bool attrValue_p) |
Set attribute of type BOOL . More... | |
uint32_t | EI_API_CIP_setAttr_sint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_sint attrValue_p) |
Set attribute of type SINT . More... | |
uint32_t | EI_API_CIP_setAttr_int (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_int attrValue_p) |
Set attribute of type INT . More... | |
uint32_t | EI_API_CIP_setAttr_dint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_dint attrValue_p) |
Set attribute of type DINT . More... | |
uint32_t | EI_API_CIP_setAttr_lint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lint attrValue_p) |
Set attribute of type LINT . More... | |
uint32_t | EI_API_CIP_setAttr_usint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_usint attrValue_p) |
Set attribute of type USINT . More... | |
uint32_t | EI_API_CIP_setAttr_uint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_uint attrValue_p) |
Set attribute of type UINT . More... | |
uint32_t | EI_API_CIP_setAttr_udint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_udint attrValue_p) |
Set attribute of type UDINT . More... | |
uint32_t | EI_API_CIP_setAttr_ulint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_ulint attrValue_p) |
Set attribute of type ULINT . More... | |
uint32_t | EI_API_CIP_setAttr_real (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_real attrValue_p) |
Set attribute of type REAL . More... | |
uint32_t | EI_API_CIP_setAttr_lreal (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lreal attrValue_p) |
Set attribute of type LREAL . More... | |
uint32_t | EI_API_CIP_setAttr_shortstring (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_shortstring *pAttrValue_p) |
Set attribute of type SHORT_STRING . More... | |
uint32_t | EI_API_CIP_setAttr_byte (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_byte attrValue_p) |
Set attribute of type BYTE . More... | |
uint32_t | EI_API_CIP_setAttr_word (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_word attrValue_p) |
Set attribute of type WORD . More... | |
uint32_t | EI_API_CIP_setAttr_dword (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_dword attrValue_p) |
Set attribute of type DWORD . More... | |
uint32_t | EI_API_CIP_setAttr_lword (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lword attrValue_p) |
Set attribute of type LWORD . More... | |