![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.00.00
|
|
Go to the documentation of this file.
111 uint8_t *buf, uint32_t len) ;
127 uint8_t *buf, uint32_t len) ;
148 typedef struct Flash_Params_s {
157 typedef struct Flash_Fxns_s
170 typedef struct Flash_Attrs_s {
188 typedef struct Flash_Config_s
198 #include <board/flash/flash_nor_xspi.h>
199 #include <board/flash/flash_nor_ospi.h>
200 #include <board/flash/flash_nor_qspi.h>
void Flash_close(Flash_Handle handle)
Close flash driver.
Flash_Attrs * attrs
Definition: flash.h:190
uint32_t flashSize
Definition: flash.h:175
Flash_OpenFxn openFxn
Definition: flash.h:159
uint32_t blockCount
Definition: flash.h:176
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:95
uint32_t driverInstance
Definition: flash.h:174
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:189
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
uint32_t sectorSize
Definition: flash.h:181
Flash_Fxns * fxns
Definition: flash.h:191
uint32_t pageSize
Definition: flash.h:179
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:110
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:170
Flash_EraseFxn eraseFxn
Definition: flash.h:163
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:158
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:140
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint32_t rsv
Definition: flash.h:150
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:58
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:126
Flash_CloseFxn closeFxn
Definition: flash.h:160
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
uint32_t pageCount
Definition: flash.h:178
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:63
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint32_t blockSize
Definition: flash.h:177
uint32_t deviceId
Definition: flash.h:172
Flash_ReadFxn readFxn
Definition: flash.h:161
Flash_WriteFxn writeFxn
Definition: flash.h:162
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:83
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint32_t manufacturerId
Definition: flash.h:173
void * devDefines
Definition: flash.h:192
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint32_t sectorCount
Definition: flash.h:180
Parameters passed during Flash_open()
Definition: flash.h:148
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:53
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
void * object
Definition: flash.h:193