Module | Supported CPUs | SysConfig Support | OS support | Key features tested | Key features not tested / NOT supported |
Address Translate | M4F | YES | FreeRTOS, NORTOS | Use RAT to allow M4F access to peripheral address space | - |
Cache | R5F | YES | FreeRTOS, NORTOS | Cache write back, invalidate, enable/disable | - |
Clock | R5F, M4F | YES | FreeRTOS, NORTOS | Tick timer at user specified resolution, timeouts and delays | - |
CycleCounter | R5F, M4F | NA | FreeRTOS, NORTOS | Measure CPU cycles using CPU specific internal counters | - |
Debug | R5F, M4F | YES | FreeRTOS, NORTOS | Logging and assert to any combo of: UART, CCS, shared memory | - |
Heap | R5F, M4F | NA | FreeRTOS, NORTOS | Create arbitrary heaps in user defined memory segments | - |
Hwi | R5F, M4F | YES | FreeRTOS, NORTOS | Interrupt register, enable/disable/restore | - |
MPU | R5F, M4F | YES | FreeRTOS, NORTOS | Setup MPU and control access to address space | - |
Semaphore | R5F, M4F | NA | FreeRTOS, NORTOS | Binary, Counting Semaphore, recursive mutexs with timeout | - |
Task | R5F, M4F | NA | FreeRTOS | Create, delete tasks | - |
Timer | R5F, M4F | YES | FreeRTOS, NORTOS | Configure arbitrary timers | - |
Peripheral | Supported CPUs | SysConfig Support | Key features tested | Key features not tested / NOT supported |
ADC | R5F | YES | Single conversion (one-shot mode), interrupt mode | Continuous conversions |
CRC | R5F | NO | Only compiled | Not tested |
ECAP | R5F | NO | Only compiled | Not tested |
EPWM | R5F | YES | Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module | Tripzone module |
EQEP | R5F | NO | Only compiled | Not tested |
FSI (RX/TX) | R5F | YES | RX, TX, polling, interrupt mode, single/dual lanes | - |
GPIO | R5F, M4F | YES | Basic input/output, GPIO as interrupt | - |
I2C | R5F, M4F | YES | Master mode, basic read/write, polling and interrupt mode | Slave mode. M4F not tested due to EVM limitation |
IPC Notify | R5F, M4F | YES | Low latency IPC between RTOS/NORTOS CPUs | - |
IPC Rpmsg | R5F | YES | RPMessage protocol based IPC, All R5F and Linux A53 cores | M4F core |
MCAN | R5F | YES | RX, TX, interrupt mode | Polling mode not tested |
MCSPI | R5F, M4F | YES | Master/Slave mode, basic read/write, polling, interrupt mode | DMA mode |
MDIO | R5F | NA | Register read/write, link status and link interrupt enable API | - |
OSPI | R5F | YES | Read direct, Write indirect, Read/Write commands, DMA for read | PHY Mode, Interrupt Mode not supported yet |
Pinmux | R5F, M4F | YES | Tested with multiple peripheral pinmuxes | - |
PRUICSS | R5F | YES | Tested with Ethercat FW HAL, HDSL, EnDat | More protocols integration tests pending |
SOC | R5F, M4F | YES | lock/unlock MMRs, get CPU clock, CPU name, clock enable, set Hz | - |
Sciclient | R5F, M4F | YES | Tested with clock setup, module on/off | - |
SPINLOCK | R5F, M4F | NA | Lock, unlock HW spinlocks | - |
UART | R5F, M4F | YES | Basic read/write, polling, interrupt mode, | HW flow control not tested, DMA mode not supported |
UDMA | R5F | YES | Basic memory copy, SW trigger, Chaining, ADC | - |
ID | Head Line | Module | Reported in release | Workaround |
MCUSDK-177 | DMTimer on M4F results in 2 interrupts instead of 1 for every DM timer expiry in release mode | DPL | 7.3.0 | Use ClockP module which uses SysTick M4 timer and this does not have any issues. |
MCUSDK-180 | Bootloader: Flash_Open and other APIs in SBL fail when the bootmode is OSPI | Bootloader | 7.3.0 | Use CCS scripting or SD card based SOC init method as mentioned in userguide when running `ospi_flash_io |
MCUSDK-316 | ROV does not work with DDR being used in application | FreeRTOS | 7.3.0 | ROV cannot be used when operating from DDR |
MCUSDK-317 | OSPI: DMA reads fails after a flash write which was not block aligned | OSPI | 7.3.0 | Use non-DMA read mode or use DMA mode but always write from start of a erased block |
MCUSDK-353 | ENDAT: EnDAT diagnostic does not support multi channel. | ENDAT | 7.3.0 | Use single channel at a time. |
MCUSDK-354 | EtherCAT State Machine from EtherCAT Conformance Test fails intermittently | EtherCAT | 7.3.0 | Use debug mode library for FreeRTOS. The makefile and projectspec for this example use debug mode library by default for all configurations |