AM64x MCU+ SDK  08.00.00
Benchmark Demo with Linux on A53

Introduction

The benchmark demo showcases the capabilities of the four R5F cores as well as the A53 core. This demo is run by default when Processor SDK Linux is flashed to SD card. Different R5F benchmarks will run on each of the four R5F cores. There are four options available for each benchmark. Users can switch the options using the drop-down menu in the GUI to view performance of R5F with each option.

The mapping of R5F core to the benchmark that is run is shown below

R5 Core Benchmark Default Option Description
R5F Core 0 (rf5ss0-0) ADC and PWM benchmark 8 Khz execution loop ADC/PWM benchmark for R5F, here we read 5 ADC samples and do 1 PWM write. NOTE: This is not enabled in current release.
R5F Core 1 (rf5ss0-1) CFFT benchmark 1Khz execution loop, 128 point CFFT CMSIS CFFT benchmark for R5F
R5F Core 2 (rf5ss1-0) FIR filtering benchmark 1 Khz execution loop, 320 point, 29-tap CMSIS FIR filtering benchmark for R5F
R5F Core 3 (rf5ss1-1) Field Oriented Control (FOC) benchmark 16 Khz execution loop CMSIS FOC benchmark for R5F

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-1 nortos
r5fss1-0 nortos
r5fss1-1 nortos
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/motor_control/benchmark_demo/

Steps to Run the Example

Hardware Prerequisites

Other than the basic EVM setup mentioned in EVM Setup, below additional HW is required to run this demo

  • PC with a web browser and wired ethernet connectivity (Windows or Linux)
  • Ethernet cables
  • Ethernet switch or ethernet router with DHCP service
  • SD card (minimum 2GB)

Build the R5F side projects

Note
The default Processor SDK Linux has prebuilt applications already, so this step can be skipped unless you have modified the demo application on R5F.
This is a system or multi-core project, so refer to system project build instructions for CCS project or makefiles when building the example.
  • When using CCS projects to build, import the system CCS project and build it using the CCS project menu (see Using SDK with CCS Projects). This will build all the dependant CPU projects as well
  • When using makefiles to build, build the system makefile using make command (see Using SDK with Makefiles). This will build all the dependant CPU makefiles as well.
  • After the build is complete the copy the below files to the SD card containing Linux filesystem in folder /lib/firmware.
    {system project output folder}/am64-main-r5f0_0-fw
    {system project output folder}/am64-main-r5f0_1-fw
    {system project output folder}/am64-main-r5f1_0-fw
    {system project output folder}/am64-main-r5f1_1-fw
    When using makefiles to build, "system project output folder", is
    ${SDK_INSTALL_PATH}/examples/motor_control/benchmark_demo/{board}/system_nortos
    When using CCS projects to build, "system project output folder", is
    ${CCS_WORKSPACE_PATH}/benchmark_demo_{board}_system_nortos/{Debug or Release}
  • NOTE, the copy step can only be done using a Linux machine since the Linux filesystem on the SD card cannot be seen on a Windows machine.

Run the demo

  • To run this demo, Linux needs to run on the Cortex A-core.
    • This typically involves flashing a prebuilt Linux filesystem (.wic file) to the SD card
    • Refer to Processor SDK Linux user guide to setup Linux on Cortex-A core.
  • Keep the EVM in POWER-OFF state.
  • Insert the SD card with Linux filesystem onto the EVM
  • Set the EVM boot mode to "SD boot mode"

SD BOOT MODE
  • Connect an ethernet cable from your ethernet switch or router to the EVM
  • Connect your PC to the same ethernet switch or router
  • Identify and setup a UART terminal console as mentioned in Setup UART Terminal
  • POWER-ON the EVM.
  • After the Linux boot completes, login as "root", then type in "ifconfig" in Linux prompt to find out the IP address for the EVM

  • On the PC, open a Internet Browser and enter in below in the address bar,
    http://{IP address of the EVM}:8081
    Example,
    http://192.168.86.198:8081
  • The following web page will show in the browser,

  • Click on the "Benchmark Demo",

  • The R5F application for each core is fixed. User can change the Options for each core, then click LOAD to refresh the statistics

Sample Output

Shown below is a sample output when the application is run.