This example demonstrates the UART RX and TX operation by echoing char that it recieves, configured in blocking, interrupt mode of operation. When user types 'quit', the application ends.
This example shows the usage of UART Api's which receives one character at a time and echos back the same to the console using UART_write.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos | |
m4fss0-0 nortos | |
Toolchain | ti-arm-clang |
Board | am64x-evm |
Example folder | examples/drivers/uart/uart_echo |
Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to type characters and then enter and type 'quit' to exit from the application.
CCS Console:
UART Console: