Features Supported
- APIs to create binary and counting semaphore's
- APIs to create mutual exclusion semaphore
- Nesting of mutual exclusion semaphores
- Priority inheritance when supported by the underlying OS
Features NOT Supported
NA
Important Usage Guidelines
- SemaphoreP_post can be called from ISR as well as task context
- SemaphoreP_pend should not be called within ISR context. It can be called from task context.
- SemaphoreP_pend will block until the user specific timeout ticks have expired or semaphore is acquired.
- In baremtal case, there is only a single main task and that will block or spin until the ticks have elasped or semaphore acquire is successful
- In RTOS case, the current executing task will 'pend' and schedular will switch to another ready task until the ticks have elasped or semaphore acquire is successful
- In both cases ISR's are still active
- There is nothing like priority inheritance in baremetal mode
Example Usage
Include the below file to access the APIs,
Example usage to define a semaphore
#define NUM_RESOURCES (10u)
uint32_t gResource[NUM_RESOURCES];
Example usage to post a binary semaphore from a ISR
void myISR(void *args)
{
}
Example usage to create and use a mutex
Example usage to create and use a binary semaphore with timeout
int32_t status;
{
}
else
{
}
else
{
}
Example usage to create and use a counting semaphore
uint32_t resourceId = 0;
resourceId = (resourceId+1)%NUM_RESOURCES;
API
APIs for Semaphore