AM62x MCU+ SDK  12.00.00
sciclient_lpm.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2024 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
48 #ifndef SCICLIENT_LPM_H_
49 #define SCICLIENT_LPM_H_
50 
51 /* ========================================================================== */
52 /* Include Files */
53 /* ========================================================================== */
54 
55 #include <stdint.h>
56 
57 #ifdef __cplusplus
58 extern "C" {
59 #endif
60 
61 /* ========================================================================== */
62 /* Macros & Typedefs */
63 /* ========================================================================== */
64 
72 };
73 
74 /* ========================================================================== */
75 /* Structure Declarations */
76 /* ========================================================================== */
77 
78 /* None */
79 
80 /* ========================================================================== */
81 /* Function Declarations */
82 /* ========================================================================== */
83 
105 int32_t Sciclient_lpmSetModuleConstraint(uint32_t moduleId,
106  uint8_t state,
107  uint32_t timeout);
108 
128 int32_t Sciclient_lpmGetModuleConstraint(uint32_t moduleId,
129  uint8_t *state,
130  uint32_t timeout);
131 
152 int32_t Sciclient_lpmSetLatencyConstraint(uint16_t resumeLatency,
153  uint8_t state,
154  uint32_t timeout);
155 
172 int32_t Sciclient_lpmGetLatencyConstraint(uint16_t *resumeLatency,
173  uint8_t *state,
174  uint32_t timeout);
175 
189 int32_t Sciclient_lpmGetNextSysMode(uint32_t timeout,
190  uint8_t *sysMode);
191 
205 int32_t Sciclient_lpmGetNextHostState(uint32_t timeout,
206  uint8_t *hostState);
207 
224 int32_t Sciclient_lpmGetWakeReason(uint32_t *wakeSource, uint64_t *wakeTimestamp, uint8_t *wakePin, uint8_t *mode, uint32_t timeout);
225 
240 int32_t Sciclient_lpmSendPrepareSleepMessage(uint8_t mode, uint32_t timeout);
241 
242 #ifdef __cplusplus
243 }
244 #endif
245 
246 #endif /* #ifndef SCICLIENT_LPM_H_ */
247 
Sciclient_lpmSetLatencyConstraint
int32_t Sciclient_lpmSetLatencyConstraint(uint16_t resumeLatency, uint8_t state, uint32_t timeout)
Message to set the system resume latency constraint. This is used to set latency for waking up from l...
mode
uint8_t mode
Definition: tisci_lpm.h:1
Sciclient_lpmSetModuleConstraint
int32_t Sciclient_lpmSetModuleConstraint(uint32_t moduleId, uint8_t state, uint32_t timeout)
Message to set constraint on a module. This is used to set constraint on a module....
Sciclient_lpmSendPrepareSleepMessage
int32_t Sciclient_lpmSendPrepareSleepMessage(uint8_t mode, uint32_t timeout)
Message to send the prepare sleep.
TISCI_LPM_SYS_MODE_IO_ONLY_PLUS_DDR
@ TISCI_LPM_SYS_MODE_IO_ONLY_PLUS_DDR
Definition: sciclient_lpm.h:68
TISCI_LPM_SYS_MODE_MCU_ONLY
@ TISCI_LPM_SYS_MODE_MCU_ONLY
Definition: sciclient_lpm.h:67
TISCI_LPM_SYS_MODE_STANDBY
@ TISCI_LPM_SYS_MODE_STANDBY
Definition: sciclient_lpm.h:70
Sciclient_lpmGetWakeReason
int32_t Sciclient_lpmGetWakeReason(uint32_t *wakeSource, uint64_t *wakeTimestamp, uint8_t *wakePin, uint8_t *mode, uint32_t timeout)
Message to get the wake up information for last entered low power mode.
gLPMSysModes
gLPMSysModes
Definition: sciclient_lpm.h:65
Sciclient_lpmGetNextSysMode
int32_t Sciclient_lpmGetNextSysMode(uint32_t timeout, uint8_t *sysMode)
Message to get the next system mode.
TISCI_LPM_SYS_MODE_PARTIAL_IO
@ TISCI_LPM_SYS_MODE_PARTIAL_IO
Definition: sciclient_lpm.h:69
TISCI_LPM_SYS_MODE_NOT_SELECTED
@ TISCI_LPM_SYS_MODE_NOT_SELECTED
Definition: sciclient_lpm.h:71
Sciclient_lpmGetNextHostState
int32_t Sciclient_lpmGetNextHostState(uint32_t timeout, uint8_t *hostState)
Message to get the next host state.
state
uint32_t state
Definition: tisci_boardcfg_pm.h:1
Sciclient_lpmGetModuleConstraint
int32_t Sciclient_lpmGetModuleConstraint(uint32_t moduleId, uint8_t *state, uint32_t timeout)
Message to get the state of constraint on a Module. This request does not require the processing enti...
Sciclient_lpmGetLatencyConstraint
int32_t Sciclient_lpmGetLatencyConstraint(uint16_t *resumeLatency, uint8_t *state, uint32_t timeout)
Message to get the system resume latency constraint value.
TISCI_LPM_SYS_MODE_DEEP_SLEEP
@ TISCI_LPM_SYS_MODE_DEEP_SLEEP
Definition: sciclient_lpm.h:66